InitialConditionsEntryMethod Enumeration

NXOpen.CAE.ResponseSimulation.InitialConditions.EntryMethod is an alias for NXOpen.CAE.ResponseSimulation.InitialConditionsEntryMethod

class NXOpen.CAE.ResponseSimulation.InitialConditionsEntryMethod

Bases: object

Specifies how to define initial condition for the user customization

Enum Members

Enum Member Enum Member Description
ManualData
FromEef
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.