FrfEvaluationSettingBuilder Class

class NXOpen.CAE.ResponseSimulation.FrfEvaluationSettingBuilder

Bases: NXOpen.CAE.ResponseSimulation.ModalResultsEvaluationSettingBuilder

This is a manager to the NXOpen.CAE.ResponseSimulation.FrfEvaluationSetting class.

Object of type NXOpen.CAE.ResponseSimulation.FrfEvaluationSetting can be created and edited only through this class

To create a new instance of this class, use NXOpen.CAE.ResponseSimulation.EvaluationSettingManager.CreateFrfEvaluationSettingBuilder()

New in version NX5.0.0.

Properties

Property Description
DataLocation Returns the frequency setting
EvaluationProperty Returns the frequency setting
InputDirection Returns or sets the source direction data component
InputNode Returns or sets the source node.
ObservationNode Returns or sets the observation nodes.
OutputRequest Returns or sets the destination direction data component
OutputSettings Returns the output setting.
ResultType Returns or sets the result type
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
GetOutputElements Returns destination nodes.
GetOutputNodes Returns destination nodes.
SetOutputElements Sets destination nodes
SetOutputNodes Sets destination nodes
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Method Detail

Validate

FrfEvaluationSettingBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.