ExcitationBuilderExcitationLocationType Enumeration

NXOpen.CAE.ResponseSimulation.ExcitationBuilder.ExcitationLocationType is an alias for NXOpen.CAE.ResponseSimulation.ExcitationBuilderExcitationLocationType

class NXOpen.CAE.ResponseSimulation.ExcitationBuilderExcitationLocationType

Bases: object

the type of excitation location

Enum Members

Enum Member Enum Member Description
StaticLoad
DistributedLoad
NodalForce
EnforcedMotion
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.