EvaluationParametersAnalysisIntegrationMethod Enumeration

NXOpen.CAE.ResponseSimulation.EvaluationParameters.AnalysisIntegrationMethod is an alias for NXOpen.CAE.ResponseSimulation.EvaluationParametersAnalysisIntegrationMethod

class NXOpen.CAE.ResponseSimulation.EvaluationParametersAnalysisIntegrationMethod

Bases: object

the integration method used for transient analysis

Enum Members

Enum Member Enum Member Description
DuhameldIntegral
NewmarkBeta
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.