ElementLocation Enumeration

class NXOpen.CAE.ResponseSimulation.ElementLocation

Bases: object

Specifies element locations Enum Members

Enum Member Enum Member Description
Both
Centroid
Corners
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.