DataLocationShell Enumeration

NXOpen.CAE.ResponseSimulation.DataLocation.Shell is an alias for NXOpen.CAE.ResponseSimulation.DataLocationShell

class NXOpen.CAE.ResponseSimulation.DataLocationShell

Bases: object

Specifies the location for shell

Enum Members

Enum Member Enum Member Description
Top
Bottom
Middle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.