DDAMExcitationMountingType Enumeration

NXOpen.CAE.ResponseSimulation.DDAMExcitation.MountingType is an alias for NXOpen.CAE.ResponseSimulation.DDAMExcitationMountingType

class NXOpen.CAE.ResponseSimulation.DDAMExcitationMountingType

Bases: object

Specifies the mounting type

Enum Members

Enum Member Enum Member Description
Hull
Duck
ShellPlating
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.