DDAMComponentDataLoadingType Enumeration

NXOpen.CAE.ResponseSimulation.DDAMComponentData.LoadingType is an alias for NXOpen.CAE.ResponseSimulation.DDAMComponentDataLoadingType

class NXOpen.CAE.ResponseSimulation.DDAMComponentDataLoadingType

Bases: object

Specifies the loading type

Enum Members

Enum Member Enum Member Description
Vertical
Athwartship
ForeAndAft
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.