CSDExcitationCorrelationType Enumeration

NXOpen.CAE.ResponseSimulation.CSDExcitation.CorrelationType is an alias for NXOpen.CAE.ResponseSimulation.CSDExcitationCorrelationType

class NXOpen.CAE.ResponseSimulation.CSDExcitationCorrelationType

Bases: object

Represents the correlation type.

Enum Members

Enum Member Enum Member Description
PhaseAngle
TimeDelay
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.