Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
GetVertices | Returns the resultant vertices |
Method Detail¶
Dispose¶
-
RelatedVertexMethod.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetVertices¶
-
RelatedVertexMethod.
GetVertices
¶ Returns the resultant vertices
Signature
GetVertices()
Returns: Resultant vertices Return type: list of NXOpen.CAE.CAEVertex
New in version NX6.0.4.
License requirements: None.