Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetElementFaces | Returns the resultant element faces |
GetFeElemFaces | Returns the resultant element faces |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
Method Detail¶
Dispose¶
-
RelatedElemFaceMethod.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetElementFaces¶
-
RelatedElemFaceMethod.
GetElementFaces
¶ Returns the resultant element faces
Signature
GetElementFaces()
Returns: Return type: list of NXOpen.CAE.SetObject
New in version NX6.0.4.
Deprecated since version NX11.0.2: Use
NXOpen.CAE.RelatedElemFaceMethod.GetFeElemFaces()
.License requirements: None.
GetFeElemFaces¶
-
RelatedElemFaceMethod.
GetFeElemFaces
¶ Returns the resultant element faces
Signature
GetFeElemFaces()
Returns: Resultant element faces Return type: list of NXOpen.CAE.FEElemFace
New in version NX11.0.2.
License requirements: None.