QueryCurveManager Class¶
-
class
NXOpen.CAE.
QueryCurveManager
¶ Bases:
object
Provides methods for managing the query curves.
To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateQueryCurveBuilder | Creates a builder for query curve create command |
Method Detail¶
CreateQueryCurveBuilder¶
-
QueryCurveManager.
CreateQueryCurveBuilder
¶ Overloaded method CreateQueryCurveBuilder
CreateQueryCurveBuilder()
CreateQueryCurveBuilder(querycurve)
-------------------------------------
Creates a builder for query curve create command
Signature
CreateQueryCurveBuilder()
Returns: Return type: NXOpen.CAE.QueryCurveBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------
Creates builder for creating or editing query curves
Signature
CreateQueryCurveBuilder(querycurve)
Parameters: querycurve ( NXOpen.CAE.QueryCurve
) – The input QueryCurve to be edited or CAE.QueryCurve.NULL when creating a new QueryCurveReturns: Return type: NXOpen.CAE.QueryCurveBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
-------------------------------------