PropertyTablePropertyType Enumeration¶
NXOpen.CAE.PropertyTable.PropertyType is an alias for NXOpen.CAE.PropertyTablePropertyType
-
class
NXOpen.CAE.
PropertyTablePropertyType
¶ Bases:
object
Property Types
Enum Members
Enum Member Enum Member Description Unknown BASE_PROPERTY_TABLE_property_type_unknown String BASE_PROPERTY_TABLE_property_type_string Boolean BASE_PROPERTY_TABLE_property_type_boolean Integer BASE_PROPERTY_TABLE_property_type_integer Double BASE_PROPERTY_TABLE_property_type_double FieldWrapper BASE_PROPERTY_TABLE_property_type_field_wrapper ScalarFieldWrapper BASE_PROPERTY_TABLE_property_type_scalar_field_wrapper CoordinateSystem BASE_PROPERTY_TABLE_property_type_coordinate_system DoubleArray BASE_PROPERTY_TABLE_property_type_double_array IntegerArray BASE_PROPERTY_TABLE_property_type_integer_array PhysicalMaterial BASE_PROPERTY_TABLE_property_type_physical_material Matrix BASE_PROPERTY_TABLE_property_type_matrix ScalarTable BASE_PROPERTY_TABLE_property_type_scalar_table Text FieldExpression VectorFieldWrapper Vector Reference Point DateTime NamedPropertyTableArray SetManager NamedPropertyTable Axis CaeSection SectionOrientation SectionOffset ReferenceArray StringArray -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-