ProjectNodesToCadGeometryBuilderOperation Enumeration¶
NXOpen.CAE.ProjectNodesToCadGeometryBuilder.Operation is an alias for NXOpen.CAE.ProjectNodesToCadGeometryBuilderOperation
-
class
NXOpen.CAE.
ProjectNodesToCadGeometryBuilderOperation
¶ Bases:
object
Operations
Enum Members
Enum Member Enum Member Description Show Display information on nodes that are off the CAD geometry by more than the input tolerance Adjust Adjust nodes that are off the geometry by more than the input tolerance by projecting them on to the CAD geometry -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-