ProjectNodesToCadGeometryBuilderListingOption Enumeration¶
NXOpen.CAE.ProjectNodesToCadGeometryBuilder.ListingOption is an alias for NXOpen.CAE.ProjectNodesToCadGeometryBuilderListingOption
-
class
NXOpen.CAE.
ProjectNodesToCadGeometryBuilderListingOption
¶ Bases:
object
Listing Options
Enum Members
Enum Member Enum Member Description NotSet List nothing SummaryOnly List only Summary information All List All information on nodes that are off the CAD geometry by more than the input tolerance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-