PrimitiveRecipeMeshBuilderType Enumeration¶
NXOpen.CAE.PrimitiveRecipeMeshBuilder.Type is an alias for NXOpen.CAE.PrimitiveRecipeMeshBuilderType
-
class
NXOpen.CAE.
PrimitiveRecipeMeshBuilderType
¶ Bases:
object
Mesh primitive type
Enum Members
Enum Member Enum Member Description Sphere Sphere Primitive Plane Plane Primitive PointSet Point Set Primitive IsoPower ISO Power (ISO3744) Primitive BoxSurface Box Surface Primitive BoxSolid Box Solid Primitive Circle Circle Primitive Line Line Primitive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-