PreTestSolutionBuilder Class¶
-
class
NXOpen.CAE.
PreTestSolutionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.PreTestSolution
builderTo create a new instance of this class, use
NXOpen.CAE.PreTestSolutionCollection.CreatePretestBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
HighFrequencyCutoff | Returns or sets the high-frequency cutoff |
HighFrequencyFilteringMode | Returns or sets the high-frequency filtering option |
LowFrequencyCutoff | Returns or sets the low-frequency cutoff |
LowFrequencyFilteringMode | Returns or sets the low-frequency filtering option |
Name | Returns or sets the pre-test name |
Solution | Returns or sets the pre-test working solution |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreTestSolutionBuilderModeConversionType Enumeration | Enum type for the complex mode conversion settings |
Property Detail¶
HighFrequencyCutoff¶
-
PreTestSolutionBuilder.
HighFrequencyCutoff
¶ Returns or sets the high-frequency cutoff
-------------------------------------
Getter Method
Signature
HighFrequencyCutoff
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HighFrequencyCutoff
Parameters: cutoffFrequency (float) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
HighFrequencyFilteringMode¶
-
PreTestSolutionBuilder.
HighFrequencyFilteringMode
¶ Returns or sets the high-frequency filtering option
-------------------------------------
Getter Method
Signature
HighFrequencyFilteringMode
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HighFrequencyFilteringMode
Parameters: highFrequencyFilteringMode (bool) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
LowFrequencyCutoff¶
-
PreTestSolutionBuilder.
LowFrequencyCutoff
¶ Returns or sets the low-frequency cutoff
-------------------------------------
Getter Method
Signature
LowFrequencyCutoff
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowFrequencyCutoff
Parameters: cutoffFrequency (float) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
LowFrequencyFilteringMode¶
-
PreTestSolutionBuilder.
LowFrequencyFilteringMode
¶ Returns or sets the low-frequency filtering option
-------------------------------------
Getter Method
Signature
LowFrequencyFilteringMode
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowFrequencyFilteringMode
Parameters: lowFrequencyFilteringMode (bool) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Name¶
-
PreTestSolutionBuilder.
Name
¶ Returns or sets the pre-test name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Solution¶
-
PreTestSolutionBuilder.
Solution
¶ Returns or sets the pre-test working solution
-------------------------------------
Getter Method
Signature
Solution
Returns: Return type: NXOpen.CAE.SimSolution
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Solution
Parameters: solution ( NXOpen.CAE.SimSolution
) –New in version NX7.5.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
Validate¶
-
PreTestSolutionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.