PreTestSensorSelectionDofSetCollection Class¶
-
class
NXOpen.CAE.
PreTestSensorSelectionDofSetCollection
¶ Bases:
object
Represents a collection of sensor selection configuration.
Contains two objects: the candidate dof set and the required dof set. To obtain an instance of this class, refer to
NXOpen.CAE.PreTestSensorSelectionControl
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds a sensor selection configuration with specified name |
Method Detail¶
FindObject¶
-
PreTestSensorSelectionDofSetCollection.
FindObject
¶ Finds a sensor selection configuration with specified name
Signature
FindObject(name)
Parameters: name (str) – dof set name, either “Candidate DOF” or “Required DOF” Returns: dof set Return type: NXOpen.CAE.PreTestDofSet
New in version NX7.5.0.
License requirements: None.