PreTestExciterConfigBuilder Class¶
-
class
NXOpen.CAE.
PreTestExciterConfigBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.PreTestExciterConfig
builderTo create a new instance of this class, use
NXOpen.CAE.PreTestSolutionCollection.CreateExciterConfigBuilder()
Default values.
Property Value DampingRatio 1.0 MethodChoice AutomaticNmif NmifThreshold 0.3 OffAxisAngleChoice None New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DampingRatio | Returns or sets the damping ratio |
MethodChoice | Returns or sets the exciter selection method |
Name | Returns or sets the name |
NmifThreshold | Returns or sets the damping ratio |
OffAxisAngleChoice | Returns or sets the off axis angle choice |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreTestExciterConfigBuilderMethodChoiceType Enumeration | Selected method for the exciter selection |
PreTestExciterConfigBuilderOffAxisAngleChoiceType Enumeration | Selected off axis angle for the exciter selection |
Property Detail¶
DampingRatio¶
-
PreTestExciterConfigBuilder.
DampingRatio
¶ Returns or sets the damping ratio
-------------------------------------
Getter Method
Signature
DampingRatio
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DampingRatio
Parameters: dampingRatio (float) – New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
MethodChoice¶
-
PreTestExciterConfigBuilder.
MethodChoice
¶ Returns or sets the exciter selection method
-------------------------------------
Getter Method
Signature
MethodChoice
Returns: Return type: NXOpen.CAE.PreTestExciterConfigBuilderMethodChoiceType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodChoice
Parameters: algorithmChoice ( NXOpen.CAE.PreTestExciterConfigBuilderMethodChoiceType
) –New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
Name¶
-
PreTestExciterConfigBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: title (str) – New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
NmifThreshold¶
-
PreTestExciterConfigBuilder.
NmifThreshold
¶ Returns or sets the damping ratio
-------------------------------------
Getter Method
Signature
NmifThreshold
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NmifThreshold
Parameters: nmifThreshold (float) – New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
OffAxisAngleChoice¶
-
PreTestExciterConfigBuilder.
OffAxisAngleChoice
¶ Returns or sets the off axis angle choice
-------------------------------------
Getter Method
Signature
OffAxisAngleChoice
Returns: Return type: NXOpen.CAE.PreTestExciterConfigBuilderOffAxisAngleChoiceType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffAxisAngleChoice
Parameters: offAxisAngleChoice ( NXOpen.CAE.PreTestExciterConfigBuilderOffAxisAngleChoiceType
) –New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
Validate¶
-
PreTestExciterConfigBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.