PostTarget Enumeration

NXOpen.CAE.Post.Target is an alias for NXOpen.CAE.PostTarget

class NXOpen.CAE.PostTarget

Bases: object

Target operators

Enum Members

Enum Member Enum Member Description
FreeFacees
Volume
CuttingPlane
AxisSymmetry3D
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.