PostStyle Enumeration

NXOpen.CAE.Post.Style is an alias for NXOpen.CAE.PostStyle

class NXOpen.CAE.PostStyle

Bases: object

Fringe styles

Enum Members

Enum Member Enum Member Description
SmoothContours
BandedContours
Elements
IsoLines
IsoSurfaces
Cubes
Spheres
Arrows
Tensors
Streamlines
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.