PostStreamlineSynchronization Enumeration

NXOpen.CAE.Post.StreamlineSynchronization is an alias for NXOpen.CAE.PostStreamlineSynchronization

class NXOpen.CAE.PostStreamlineSynchronization

Bases: object

Synchronization options for streamlines

Enum Members

Enum Member Enum Member Description
Upstream
Downstream
SeedPoint
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.