PostStreamlineDirection Enumeration

NXOpen.CAE.Post.StreamlineDirection is an alias for NXOpen.CAE.PostStreamlineDirection

class NXOpen.CAE.PostStreamlineDirection

Bases: object

Direction options for streamline extraction

Enum Members

Enum Member Enum Member Description
Upstream
Downstream
Both
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.