PostSpectrum Enumeration

NXOpen.CAE.Post.Spectrum is an alias for NXOpen.CAE.PostSpectrum

class NXOpen.CAE.PostSpectrum

Bases: object

colorbar spectrums

Enum Members

Enum Member Enum Member Description
Structural
Thermal
GrayScale
StopLight
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.