PostScenarioVariantType Enumeration¶
-
class
NXOpen.CAE.
PostScenarioVariantType
¶ Bases:
object
The data type of a CAE.PostScenarioVariant Value Enum Members
Enum Member Enum Member Description Unary an empty value Boolean a boolean value Integer an integer number Double a real number Complex a complex number String an ASCII character string UnicodeString a Unicode UTF-8 character string Vector3d a 3D vector Component a component ModeDescription a mode number and frequency -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-