PostScenarioVariantComponent Enumeration¶
-
class
NXOpen.CAE.
PostScenarioVariantComponent
¶ Bases:
object
Components of vectors or tensors. Enum Members
Enum Member Enum Member Description Magnitude request the magnitude of a 3D vector Scalar represents that the data is scalar X X component of a 3D vector Y Y component of a 3D vector Z Z component of a 3D vector Xx XX component of a tensor Yy YY component of a tensor Zz ZZ component of a tensor Xy XY component of a tensor Xz XZ component of a tensor Yx YX component of a tensor Yz YZ component of a tensor Zx ZX component of a tensor Zy ZY component of a tensor -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-