PostScenarioParameters Class¶
-
class
NXOpen.CAE.
PostScenarioParameters
¶ Bases:
NXOpen.TransientObject
The class represents the
NXOpen.CAE.PostScenarioParameters
used to instanciate aNXOpen.CAE.PostScenarioBuilder
.To create a new instance of this class, use
NXOpen.CAE.PostScenarioManager.NewPostScenarioParameters()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DataSource | Returns or sets the data source object to be processed by the post scenario. |
ScenarioDescriptor | Returns or sets the scenario descriptor used by the post scenario. |
ViewPortIndex | Returns or sets the index of a view port on the main graphic window, on which the plot graph will be shown. |
Methods¶
Method | Description |
---|---|
Dispose | Destroys the object |
SetPreferredDataSources | Set preferred Data Sources to influence the default configuration of a scenario. |
Property Detail¶
DataSource¶
-
PostScenarioParameters.
DataSource
¶ Returns or sets the data source object to be processed by the post scenario.
-------------------------------------
Getter Method
Signature
DataSource
Returns: Return type: NXOpen.CAE.IPostScenarioDataSource
New in version NX11.0.0.
Deprecated since version NX12.0.0: Data Sources are now added through
CAE.PostScenarioManager.DataSources()
. Alternatively,CAE.PostScenarioParameters.SetPreferredDataSources()
can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
DataSource
Parameters: dataSource ( NXOpen.CAE.IPostScenarioDataSource
) –New in version NX11.0.0.
Deprecated since version NX12.0.0: Data Sources are now added through
CAE.PostScenarioManager.DataSources()
. Alternatively,CAE.PostScenarioParameters.SetPreferredDataSources()
can be used to configure the default configuration of a scenario. Setting this attribute has the same effect as SetPreferredDataSources(value).License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ScenarioDescriptor¶
-
PostScenarioParameters.
ScenarioDescriptor
¶ Returns or sets the scenario descriptor used by the post scenario.
-------------------------------------
Getter Method
Signature
ScenarioDescriptor
Returns: Return type: NXOpen.CAE.PostScenarioDescriptor
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ScenarioDescriptor
Parameters: scenarioDesc ( NXOpen.CAE.PostScenarioDescriptor
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ViewPortIndex¶
-
PostScenarioParameters.
ViewPortIndex
¶ Returns or sets the index of a view port on the main graphic window, on which the plot graph will be shown.
-------------------------------------
Getter Method
Signature
ViewPortIndex
Returns: Return type: int New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ViewPortIndex
Parameters: viewPortIndex (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
Dispose¶
-
PostScenarioParameters.
Dispose
¶ Destroys the object
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
SetPreferredDataSources¶
-
PostScenarioParameters.
SetPreferredDataSources
¶ Set preferred Data Sources to influence the default configuration of a scenario.
If the default configuration of a scenario is known to be overridden later in the program, there is no need to call this method. Setting a single preferred data source enables the behaviour from version 11.0.0.
Signature
SetPreferredDataSources(dataSources)
Parameters: dataSources (list of NXOpen.CAE.DataSource
) – The data sources can be retrieved fromCAE.PostScenarioManager.DataSources()
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)