PostScenarioInputDefinition Class¶
-
class
NXOpen.CAE.
PostScenarioInputDefinition
¶ Bases:
NXOpen.TaggedObject
Represents an Input Definition, part of a
NXOpen.CAE.PostScenarioDescriptor
.An input definition is an interpretation of data by a scenario. When building a scenario, selecting an input definition, on top of a data source’s
NXOpen.CAE.PostScenarioDataDefinition
, results in the scenario interpreting the available data in a specific way in order to post-process the data.Not support KF.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Name | Returns the name of this Input Definition. |
Tag | Returns the Tag for this object. |
Visualizations | The collection of visualizations (NXOpen.CAE.PostScenarioVisualizationDefinition ) available for this Scenario Input Definition. |
MeshDefinitions | The collection of mesh definitions (NXOpen.CAE.PostScenarioMeshDefinition ) available for this Scenario Input Definition. |
Methods¶
Property Detail¶
Name¶
-
PostScenarioInputDefinition.
Name
¶ Returns the name of this Input Definition.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
Visualizations¶
-
PostScenarioInputDefinition.
Visualizations
¶ The collection of visualizations (
NXOpen.CAE.PostScenarioVisualizationDefinition
) available for this Scenario Input Definition.Signature
Visualizations
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.PostScenarioVisualizationCollection
MeshDefinitions¶
-
PostScenarioInputDefinition.
MeshDefinitions
¶ The collection of mesh definitions (
NXOpen.CAE.PostScenarioMeshDefinition
) available for this Scenario Input Definition.Signature
MeshDefinitions
New in version NX12.0.0.
Returns: Return type: NXOpen.CAE.PostScenarioMeshDefinitionCollection