PostScenarioAvailableDescriptorCollection Class¶
-
class
NXOpen.CAE.
PostScenarioAvailableDescriptorCollection
¶ Bases:
object
A collection of :py:class:`NXOpen.CAE.PostScenarioDescriptor`s.
These descriptors are used in Application Specific Post Processing to create a post processing scenario. A descriptor defines how data is retrieved from a
NXOpen.CAE.DataSource
, how it is processed, and how it is displayed throughNXOpen.CAE.PostScenarioBuilder.Visualization()
. See alsoNXOpen.CAE.PostScenarioBuilder
. To obtain an instance of this class, refer toNXOpen.CAE.PostScenarioManager
New in version NX12.0.0.
Method Detail¶
Find¶
-
PostScenarioAvailableDescriptorCollection.
Find
¶ Finds an input definition with a certain name.
Signature
Find(name)
Parameters: name (str) – name of the descriptor Returns: Return type: NXOpen.CAE.PostScenarioDescriptor
New in version NX12.0.0.
License requirements: None.