PostScale Enumeration

NXOpen.CAE.Post.Scale is an alias for NXOpen.CAE.PostScale

class NXOpen.CAE.PostScale

Bases: object

Colorbar scales

Enum Members

Enum Member Enum Member Description
Automatic
Linear
Logarithmic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.