PostProcessingSession Class¶
-
class
NXOpen.CAE.
PostProcessingSession
¶ Bases:
object
This is the class representing a
NXOpen.CAE.PostProcessingSession
.Not support KF.
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateBuilder | Creates a NXOpen.CAE.PostProcessingSessionApplicator . |
ExportToFile | Exports the Post Processing Session to an external file |
Method Detail¶
CreateBuilder¶
-
PostProcessingSession.
CreateBuilder
¶ Creates a
NXOpen.CAE.PostProcessingSessionApplicator
.This builder is used to create or edit a post processing session.
Signature
CreateBuilder(part)
Parameters: part ( NXOpen.CAE.CaePart
) –Returns: Return type: NXOpen.CAE.PostProcessingSessionApplicator
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ExportToFile¶
-
PostProcessingSession.
ExportToFile
¶ Exports the Post Processing Session to an external file
Signature
ExportToFile(part, filePath)
Parameters: - part (
NXOpen.CAE.CaePart
) – - filePath (str) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- part (