PostNodeValueSharingCriterion Enumeration

NXOpen.CAE.Post.NodeValueSharingCriterion is an alias for NXOpen.CAE.PostNodeValueSharingCriterion

class NXOpen.CAE.PostNodeValueSharingCriterion

Bases: object

Criteria for value sharing of extracted data at a graph point

Enum Members

Enum Member Enum Member Description
Average
Minimum
Maximum
Sum
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.