PostMarkRenderStyle Enumeration

NXOpen.CAE.Post.MarkRenderStyle is an alias for NXOpen.CAE.PostMarkRenderStyle

class NXOpen.CAE.PostMarkRenderStyle

Bases: object

Mark render styles

Enum Members

Enum Member Enum Member Description
Line
Solid
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.