PostMarkColor Enumeration

NXOpen.CAE.Post.MarkColor is an alias for NXOpen.CAE.PostMarkColor

class NXOpen.CAE.PostMarkColor

Bases: object

Mark color options

Enum Members

Enum Member Enum Member Description
ResultValue
Specified
Textcolor
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.