PostGroupVisibility Enumeration

NXOpen.CAE.Post.GroupVisibility is an alias for NXOpen.CAE.PostGroupVisibility

class NXOpen.CAE.PostGroupVisibility

Bases: object

Show hide options for user group visibiliy control

Enum Members

Enum Member Enum Member Description
ShowOnly
Show
Hide
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.