PostGraphBuilderFaceIntegralOption Enumeration

NXOpen.CAE.PostGraphBuilder.FaceIntegralOption is an alias for NXOpen.CAE.PostGraphBuilderFaceIntegralOption

class NXOpen.CAE.PostGraphBuilderFaceIntegralOption

Bases: object

weighted Average/ Integral calculation based on weighted average by on selection of Face

Enum Members

Enum Member Enum Member Description
Area
Volume
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.