PostGraphBuilderEntityType Enumeration

NXOpen.CAE.PostGraphBuilder.EntityType is an alias for NXOpen.CAE.PostGraphBuilderEntityType

class NXOpen.CAE.PostGraphBuilderEntityType

Bases: object

types of the entity objects which are selected

Enum Members

Enum Member Enum Member Description
Node
Element
Point
Edge
Face
Body
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.