PostGraphBuilderEdgeIntegralOption Enumeration

NXOpen.CAE.PostGraphBuilder.EdgeIntegralOption is an alias for NXOpen.CAE.PostGraphBuilderEdgeIntegralOption

class NXOpen.CAE.PostGraphBuilderEdgeIntegralOption

Bases: object

weighted Average / Integral calculation based on weighted average by on selection of Edge

Enum Members

Enum Member Enum Member Description
Length
Area
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.