PostGraphAlongPathBuilderCoordinateSysAxis Enumeration¶
NXOpen.CAE.PostGraphAlongPathBuilder.CoordinateSysAxis is an alias for NXOpen.CAE.PostGraphAlongPathBuilderCoordinateSysAxis
-
class
NXOpen.CAE.
PostGraphAlongPathBuilderCoordinateSysAxis
¶ Bases:
object
options for defining the specific coordinate system axis to be used
Enum Members
Enum Member Enum Member Description FirstAxis SecondAxis ThirdAxis -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-