PostGraphAcrossIterationsBuilderIterationLabelingOption Enumeration

NXOpen.CAE.PostGraphAcrossIterationsBuilder.IterationLabelingOption is an alias for NXOpen.CAE.PostGraphAcrossIterationsBuilderIterationLabelingOption

class NXOpen.CAE.PostGraphAcrossIterationsBuilderIterationLabelingOption

Bases: object

Defines the Iteration labeling options

Enum Members

Enum Member Enum Member Description
Value
Id
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.