PostGraphAcrossIterationsBuilderCombinationMethod Enumeration

NXOpen.CAE.PostGraphAcrossIterationsBuilder.CombinationMethod is an alias for NXOpen.CAE.PostGraphAcrossIterationsBuilderCombinationMethod

class NXOpen.CAE.PostGraphAcrossIterationsBuilderCombinationMethod

Bases: object

Defines the methods that can be used to combine multiple values into a single value

Enum Members

Enum Member Enum Member Description
Average
Minimum
Maximum
Sum
Difference
WeightedAverage
Integral
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.