PostFormat Enumeration

NXOpen.CAE.Post.Format is an alias for NXOpen.CAE.PostFormat

class NXOpen.CAE.PostFormat

Bases: object

Colorbar format

Enum Members

Enum Member Enum Member Description
Auto
FixedPoint
Scientific
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.