PostAnnotationTextAlignment Enumeration

NXOpen.CAE.PostAnnotation.TextAlignment is an alias for NXOpen.CAE.PostAnnotationTextAlignment

class NXOpen.CAE.PostAnnotationTextAlignment

Bases: object

Annotation text alignment

Enum Members

Enum Member Enum Member Description
Left
Right
Center
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.