PostAnnotationStyle Enumeration

NXOpen.CAE.PostAnnotation.Style is an alias for NXOpen.CAE.PostAnnotationStyle

class NXOpen.CAE.PostAnnotationStyle

Bases: object

Annotation styles

Enum Members

Enum Member Enum Member Description
Box
BoxWithLeader
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.