PostAnimationControl Enumeration

NXOpen.CAE.Post.AnimationControl is an alias for NXOpen.CAE.PostAnimationControl

class NXOpen.CAE.PostAnimationControl

Bases: object

Animation controls

Enum Members

Enum Member Enum Member Description
Back
Next
Play
Pause
Stop
SetFrame
FullCycle
Delay
Streamline
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.