PostAbcissa Enumeration

NXOpen.CAE.Post.Abcissa is an alias for NXOpen.CAE.PostAbcissa

class NXOpen.CAE.PostAbcissa

Bases: object

Abcissa types for graph

Enum Members

Enum Member Enum Member Description
Uneven
Even
Sequenced
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.