OrderedFeatureEdgeNodeMethod Class¶
-
class
NXOpen.CAE.
OrderedFeatureEdgeNodeMethod
¶ Bases:
NXOpen.SelectionMethod
Represents the output from the ordered feature edge node smart selector method
To obtain an instance of this class use CAE::SmartSelectionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetNodes | Returns the resultant nodes |
GetSelectedObjects | Returns the objects selected by this NXOpen.SelectionMethod . |
Method Detail¶
Dispose¶
-
OrderedFeatureEdgeNodeMethod.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetNodes¶
-
OrderedFeatureEdgeNodeMethod.
GetNodes
¶ Returns the resultant nodes
Signature
GetNodes()
Returns: Resultant nodes Return type: list of NXOpen.CAE.FENode
New in version NX11.0.0.
License requirements: None.