OpenDuctMeshBuilder Class¶
-
class
NXOpen.CAE.
OpenDuctMeshBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.OpenDuctMeshBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateOpenDuctMeshBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ElementEdge | Returns the selected element edge(s) |
ElementType | Returns the element type |
PropertyTable | Returns the Open Duct Mesh property table The property table contains the parameters needed for the Mesh Refinement |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AutomaticElementSize | The creation of automatic element size |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ElementEdge¶
-
OpenDuctMeshBuilder.
ElementEdge
¶ Returns the selected element edge(s)
-------------------------------------
Getter Method
Signature
ElementEdge
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX12.0.0.
License requirements: None.
ElementType¶
-
OpenDuctMeshBuilder.
ElementType
¶ Returns the element type
-------------------------------------
Getter Method
Signature
ElementType
Returns: Return type: NXOpen.CAE.ElementTypeBuilder
New in version NX12.0.0.
License requirements: None.
PropertyTable¶
-
OpenDuctMeshBuilder.
PropertyTable
¶ Returns the Open Duct Mesh property table The property table contains the parameters needed for the Mesh Refinement
-------------------------------------
Getter Method
Signature
PropertyTable
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX12.0.0.
License requirements: None.
Method Detail¶
AutomaticElementSize¶
-
OpenDuctMeshBuilder.
AutomaticElementSize
¶ The creation of automatic element size
Signature
AutomaticElementSize()
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Validate¶
-
OpenDuctMeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.