OneDimensionalElementSplitBuilderSplitMethodType Enumeration

NXOpen.CAE.OneDimensionalElementSplitBuilder.SplitMethodType is an alias for NXOpen.CAE.OneDimensionalElementSplitBuilderSplitMethodType

class NXOpen.CAE.OneDimensionalElementSplitBuilderSplitMethodType

Bases: object

represents the split method types

Enum Members

Enum Member Enum Member Description
NumberElement by number of elements
LengthElement by length of elements
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.