NodesRepositionBuilder Class¶
-
class
NXOpen.CAE.
NodesRepositionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.NodesRepositionBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateNodesRepositionBuilder()
New in version NX6.0.2.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetNodePosition | Set the new absolute postion for the input node. |
SetNodePositions | Set the new absolute postions for an array of input nodes. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
SetNodePosition¶
-
NodesRepositionBuilder.
SetNodePosition
¶ Set the new absolute postion for the input node.
New position will only take affect when Commit is done.
Signature
SetNodePosition(fenode, position)
Parameters: - fenode (
NXOpen.CAE.FENode
) –NXOpen.CAE.FENode
input node - position (
NXOpen.Point3d
) – new absolute position of node
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
- fenode (
SetNodePositions¶
-
NodesRepositionBuilder.
SetNodePositions
¶ Set the new absolute postions for an array of input nodes.
New position will only take affect when Commit is done.
Signature
SetNodePositions(fenodes, positions)
Parameters: - fenodes (list of
NXOpen.CAE.FENode
) – FENodes - positions (list of
NXOpen.Point3d
) – FENodes positions
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
- fenodes (list of
Validate¶
-
NodesRepositionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.